SCM Group

Sector: Woodworking Machinery

A strong working relationship lasting in excess of 20 years, has brought mutual benefits for both SCM Group and Camozzi Automation.

SCM Group

Source

Profitable collaboration between Camozzi and Scm (September - October 2020) 

If before it took almost twenty minutes to bring the air up to temperature and start edging, now everything is ready in less than one hundred seconds.

Nicolò Gianesini 
Engineer of the SCM Group technical department

Find out more
De Lama De Lama
De Lama

Sector: Machinery and equipment production for the pharmaceutical industry

Customised machines for sterilisation, washing and other processes, that are also compact due to the reduced size of the components used. 

Tewes-Bis
Tewes-Bis

Sector: Production of machinery and equipment for the dairy industry

The cheese production line is excellent in terms of quality, performance and reliability, thanks to the implementation of an electromechanical solution able to perfectly control the cutting speed, stroke and force while meeting stringent demands for hygiene and corrosion resistance when in contact with cleaning media.

Bonetto Automation
Bonetto Automation

Sector: Assembly, Robotics and Packaging for the industrial and medical sectors

Bonetto's ambitious plans for growth in the medical field have given rise to the development of a platform of highly standardised machines configured to cater to the end customer's needs. An interesting example is a recently-automated system for the production of pre-filled test tubes, realised with the support of Camozzi.

Open Frame Controller regelt perfekten Schliff der Skier im Reichmann Automat
Reichmann & Sohn

Sector: Machine tools and manufacturing systems

Proportional control for perfect grinding.
On Reichmann & Sohn grinding machines, the Open Frame Controller with its intelligent control system provides easy operation and ensures perfect grinding for skis and snowboards.

Rolfo SpA
Rolfo SpA

Sector: Transportation
Vehicle Category: Truck & Trailer

Small components play a critical role in the transportation of valuable loads

Schraubautomat mit Serie 5E Linearachse
Stein-Automationstechnik

Sector: Woodworking Machinery

Linear drives carve out a niche
Electro-mechanical technology from Camozzi Automation has increased speed and precision of Stein-Automationstechnik’s screwdriving system.

Tecno Meccanica
Tecno Meccanica

Sector: Food Industry

The new ham massage system of Tecno Meccanica integrates advanced Camozzi Automation components, resulting in significant product quality benefits.

Horsch Leeb
Horsch Leeb

Sector: Transportation
Vehicle Category: Off-Highway

In collaboration with the agricultural machine manufacturer Horsch Leeb, Camozzi Automation has developed chemical resistant pneumatic fittings for the airbrake system of a crop sprayer.

SCM Group
SCM Group

Sector: Woodworking Machinery

A strong working relationship lasting in excess of 20 years, has brought mutual benefits for both SCM Group and Camozzi Automation.

C&C Flexo
C&C Flexo

Sector: Printing & Paper 

Thanks to an innovative solution for managing pressure inside pneumatic cylinders, C&C Flexo produces high-performance flexographic printing machines, capable of ensuring a constant quality level of the finished product.

Fromm Packaging Automation
Fromm Packaging Automation

Sector: Packaging 

Our continuous quest for best performance begins by enlisting skilled component and systems suppliers whose expertise can optimise production cycles.

Sagicofim
Sagicofim

Sector: Filtering Systems 

The Series LR servo valve of Camozzi ensures the perfect operation of a new automatic testing system made by Sagicofim to check safety canisters for filtering devices.